Hi,
In datasheet of CC1020 I read "In NRZ mode the maximum modulating signal occurs when transmitting a 0-1-0 sequence. In both Manchester and NRZ mode 2∙fm is then equal to the programmed baud rate."
I don't get it for the NRZ, while it make sense for Manchester (because the programmed baudrate is referred to RF side, therefore not on the bitrate itself which is halved). My explanation for the NRZ is because the modulating signal have a doubled period compared to bitrate used, due to the double transition needed. Therefore tha maximum modulating frequency is always half the bitrate.
Am I correct?
Thanks!