I have a configuration for the CC1101 that I would like to use with the sniffer using smartRF however getting the configuration to work perfectly seems to be a arduous (trial and error). Is their a clean way to do this? I have a configuration I did before but frequency etc has changed. It would be VERY helpful to be able to take the smartRF configuration for a CC1101 (26mhz) and mostly migrate it to the CC1111 without guessing at settings.
It seems a bit too much trial and error to migrate the configuration. I prefer to do so in a more effective (efficient too) manner. As I have numerous frequency allocations etc. I have to deal with and this... is a pain to do for each change.
Suggestions very welcome (and yes I've already attempted to do it a few times). If necessary I can post my smartRF configuration for the CC1101 and the C1111 etc.
Thanks