I am using CC1120 EM with MSP430F5529 Launchpad.
I have two questions: -
Q1. In SimpliciTI TI Wiki link it mention that Simpliciti stack supports MSP430F5529 Launchpad and CC1120. However, I cannot find relevant details is the release and cannot use this combo. I am stuck and do not know how to proceed if there is not going to be any support. I also searched e2e but could not find detailed answer/clarity.
Q2. I am not able to communicate to CC1120 using SPI through MSP430F5529 Launchpad (using Wired board). Can you provide some working code example for SPI communication please?
Current Issue is, MISO line behaves weirdly. Do I need to use pull up on MISO line? Is MISO line drive not enough? In a continuous data read operation on SPI MISO stays low by default and toggles when SPI clk arrives. As far as I know MISO should stay high by default and only goes low when CSn goes low. Am I correct? Again, If I connect CCdebugger to CC1120EM card, it works fine. I do not know what is going wrong and how do I fix it.
Thanks,
Abhijit