Other Parts Discussed in Thread: CC2420
Hi,
The CC2420 datasheet defines current draw for different states as follows:
Power Down mode: 20 uA
Idle mode: 426 uA
Receive mode: 18.8 mA
Transmit mode: 17.4 mA (at 0 dBm)
Do Receive/Transmit correspond to the state when the transceiver is active and actually receiving/transmitting a packet OR just when the transceiver is active i.e. receiver/transmitter is ON?
If its the second case, what does Idle state refer to?
Thanks.