This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yann -
this transponder is not an ISO standard device and TI does not support it as such.
the closest device TI offers which is ISO standard are these: ,
, reader IC to use would be the TMS3705 and reader modules would be RI-STU-MRD2 (in DIL or SMD form)
speed of detection will be about 70mSec and to get 5cm should be no problem, usually ISO standard devices like what we offer here get roughly twice the distance of 125kHz tags.
how much room do you have for antenna coil? maybe you might need about a 40mm diameter coil to get 5cm or more with our 12mm tags. other options might be viable as well, like using ferrite core on the antenna which will make field smaller, but might be more compact for your application.