Hey everyone
I post few days ago on how to use the CC2650STK sensortag, and it works well, thanks !
Now i'm contacting you for a new challenge : i want Contiki to run onto the CC2650STK sensortag.
[ Contiki's documentation says it is possible. ]
First point, my hardware :still the same than the pastrs weeks : a CC2650STK and a XDS110 USB debugger.
Second point : What i've done
a - install Instant Contiki onto a virtual machine (in VBox) [step 1 only] www.contiki-os.org/start.html
b - followed the instruction to flash the tag with FLASH PROGRAMMER http://processors.wiki.ti.com/index.php/Contiki_setting_up_sw [works fine]
c - I tried to make it work directly in the VM [step 4 of the first website], because i do not want to lose time switching beetween the linux Guest InstantContiki, and the Win host to use flash programmer. So i tried and a mistake appears [the usb in the VM is ok, error doesn't come from here]
Google told me to change few things : https://github.com/contiki-os/contiki/tree/master/platform/srf06-cc26xx
Still doesn't worked ... Then google told me to install the UART drivers : https://github.com/contiki-os/contiki/tree/master/platform/cc2538dk
Obviously, i changed the numbers to have the XSD Vendor and product values, but once again it still doesn't worked.
Does anyone has an idea ?
Here is the mistake I have :
"root@<path_to_hello_world_template> # make hello-world.upload
using saved target 'srf06-cc26xx'
make: *** No rule to make target `hello-world.upload'. Stop."
Thanks
Cheers