Other Parts Discussed in Thread: TRF7960A
Hello Team,
I would need to clarify a few things about the read range of ISO15693 tags of the long range reader designed by the TI 4W HF RFID power amplifier application note with Cu tube loop antenna.
We designed longe range reader with TRF7960A and power amplifier according to app note (sloc132). The output of the amplifier is tuned with spectrum analyzer for maximum output power 4 W on the maximum PA supply voltage of 12 V. In the next step the we tune the output phase shift to 45 degrees with 50 ohm load at the output connector.
1. Is it appropriate to change the phase shift by the change of the output capacitance (C112, C113) or by the change of the inductance of coil L105 (we'd rather change the inductance)?
Next we constructed the copper tube loop antenna according to the TI HF antenna cookbook and design notes with slightly less size of 480x480 mm and with gamma matching. With vector network analyzer we tuned the antenna to 50 ohm @13,56 MHz and Q of 17. The return loss of the antenna has very similar characteristics as the antennas in app note (sloc132), it has -10 dB near the 13,15 and 13,80 MHz frequencies and -14 dB at 13,56 MHz.
One thing that I need to clarify is the Q and the bandwidth of the slightly mistuned antenna in app note. As I understand, the transmitting bandwidth is very narrow due to the very slow data rate and amplitude modulation, but the receiving bandwidth is 484 kHz on both sides from 13,56 MHz due to subcarrier frequencies.
2. Should't be the Q of the mistuned antenna lower than 20 due to the offset of the band center fequency from the 13,56 MHz?
3. How does it help to mistune the antenna to prevent the transmitter power from saturating the reiver inputs? I assumed, that with the better antenna matching (lowest return loss) the power from transmitter is more effectively transmitted by the antenna and less power returns beck to the reciver. What is the difference in this case?
We tested a read range of couple TI tags on 1W output power with following results:
circular inlay D 24 mm RI-I16-112A-03: read range of 16 cm
circular inlay D 32 mm RI-I17-112A-03: read range of 26 cm
rectangular inlay 75x45 mm RI-I02-112A-03: read range of 46 cm
I found on this forum a TI document with read ranges tested with 300 x 300 mm antenna for different tag types (7318.TI HF-I Read Ranges.ppt). When I focus on tag -CB1A CARD (large rectangle)(assume that corresponds to RI-I02-112A we used) the read ranges with 300 x 300 mm antenna TI used are even slightly better than we achieved with our 480 x 480 antenna. We tried mistune the antenna to the lower and to the higher frequencies, but with no better read ranges than mentioned earlier. Another thing is, that the increasing of the transmitter output power from 1 W to 4 W increased the read range only by 4 cm to 50 cm.
4. Can you suggest what we should to focus on to check that everything is set as it should be?
5. Is there a way to find out directly if the receiver is saturated by the transmitter signal? Is it measurable at some point of signal path?
We also tried to design "simpler" wire 1 turn loop square antennas.
The 1st has dimensions of 450 x 450 mm and is wound from 1 mm^2 stranded wire with inductance 2,66 uH.
The 2nd is 650 x 650 mm from 2,5 mm^2 stranded wire with inductance 4,37 uH.
We used both the transformer matching and capacitive matching with the same results.
With the transmitt power of 1 W and RI-I02-112A tag we achieved read range of 40 cm with the 1st smaller antenna and the read range of 45 cm with the larger 2nd antenna. We tried to mistune these antennas both to the higher and to the lower frequencies, but those were the best results.
6. Is there some problem with wire loop antennas, that would cause worse read ranges? I understand that using the wire instead the tube results in higher inductance, but with proper matching to the same impedance and Q, should be the results very similar?
Thanks and regards,
Tomas