I'm currently getting a strange issue with the cc1125 where it appears to get stuck in a continuous transmission, of 010101010 pattern, I'm not however wanting this behaviour. I'm trying to send a short message and then I#m looking for the one of the gpio pins to toggle. this was working fine at first but I decided I needed to speed up how often I send a transmission and when I did that it works for a short while and then gets stuck in this funny mode.
Spying on the line I cant see anything obvious that would indicate why this might be occurring and I'm not refilling the buffer and the buffer doesn't seem to be underflowing.
Is there some test mode that might cause this?