Other Parts Discussed in Thread: CC110L
Hello,
I worked on CC110L with the helical PCB Antenna (Design Note DN038).
I would like to redesign it to fit in a small board with a PCB thickness : 1.55mm.
In the Design Note, it is said that the length of the antenna is a main topic to match with the frequency. If I measure the length of the antenna in the DN, it is approximately 120mm. However, if I calculate the wavelength for 868MHz, it should be 8.63cm.
What is the total length I have to keep if I want to modify the value of H1 (page 3 in DN038) ?
Thank you for your help.