Hi,
I'm interested in testing Ultra Low Power Card Presence detection (as described in SLOA184), that's why I purchased two new DLP-7970ABP booster pack V4.5. The new design includes now a pin for connecting to a comparator that will regularly trigger the detection logic ,as described in SLOA184. However, this report states also that the MSP430 should be clocked with SYS_CLOCK from the TRF7970A during detection period (section 4.5, page 13), and I cannot see from the new pin layout (DLP-7970ABP Hardware update overview SLOA226) how to do it.
Anyone has suggestions ? Did anyone already implement ULP card presence detection with an MSP430 launchpad and a DLP-7970ABP booster pack ?
Best regards,