Other Parts Discussed in Thread: Z-STACK, CC2530
Hello,
After programming a CC2530 with the CC Debugger, the firmware (on the 2530) will immediately start to run. Some time after that (200ms - 2s) the operator will disconnect the programming header from the module, so it loses supply voltage quickly. I've observed that this can happen before the Vdd is checked with but during a write to flash (on Z-Stack, this is during the initialisation routines). This could possibly lead to flash corruption.
A way to prevent this is to have the programming tool keep the RESET line asserted after programming. This option is usually available, but I didn't find it in Flash Programmer tool. Is there any way to do this?
Br,
Sjef.