I have another thread going in which I am trying to establish communications with the MSP430 on a TrxEB board. I'm branching the discussion here to deal with one set of tools that is causing me some confusion. I have two questions...
I've run the "Flash Programmer" from within SmartRF Studio. When I did, it challenged the version of my set-up; I'm assuming it wasn't happy with the version in the MSP-FET430 (Question 1 - Is that correct?)
It wanted to (and I let it) update it to 3.4.3.4.
Then, I downloaded the standalone Flash Programmer and when run, it wanted 3.3.0.6. I let it do so (for giggles) but of course when I ran SmartRF Studio again, it wanted to return the device to 3.4.3.4 (which I let it, again)
Question 2 - Do I need, and is there available, the compatible stand-alone "Flash Programmer", or should I just forget about (and uninstall) the stand-alone?