This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCDebugger

Dear sir/madam

I have a CCDebugger that is not cooperating.

Let me describe the setup. I connect the CCdebugger to the custom PCB and to the Computer via USB. I press the Reset button on the CCDebugger, but the LED remains RED.


I then take the same CCDebugger connected to the same custom PCB and connect to another computer. Now the LED turns GREEN.


Both PCs are Windows 7.

When I connect the CCDebugger to both PCs, the Device Manager shows the Cebal controlled devices, indicating that the CC Debugger is connected.

Yet, the LED only turns GREEN on one of the PCs.

Anybody have any idea what the reason could be?

Thank you