I'm working on a design with a trace antenna. is there an optimal complex impedance to target for the trace antenna?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm working on a design with a trace antenna. is there an optimal complex impedance to target for the trace antenna?
Hi Mike,
Generally, you would like to see about 1uH - 1.5uH inductance. Have a look at section 10 of the users guide below which walks through tuning an antenna with XL = 0.8 + j80.8(~1uH).
Hi Mike,
I don't think that these variances would cause such a large difference in inductance. See the calculation below for a trace width of 0.3mm and 0.3254mm, which is a 1 mil difference in width. The inductance varies from 1.36uH to 1.33uH.
I think what could be more likely happening is that there is a short between two traces of the antenna coil. I have seen this happen before when the trace spacing is not adequate for the PCB manufacturer. This will essentially reduce one turn from your antenna coil, which will significantly reduce the inductance. Try to see If you can try to have a look all the way around the antenna coil trace under a microscope and see if you see any small bit of copper shorting the coil. It may be very difficult to see as it may only be a very small piece of copper.