Today I got an update in CCS for the Emulator package, new version is 6.0.83.0.
Today I experienced massive problems with the XDS110 and my custom board. When trying to download my code to the CC2640 I get the following error message:
Error connecting to the target: (Error -1265 @ 0x0) Device ID is not recognized or is not supported by driver. Confirm device and debug probe configuration is correct, or update device driver. (Emulation package 6.0.83.0).
Resetting the target device and disconnecting/reconnecting the USB cable does not help. I checked all puls forms of TDO TDI TCK and TMS, everything seems to be ok. The XDS110 connects shortly via JTAG to the CC2640 at my board and then the error message appears.
Any help?