Hi,
TRF7970A doesn't work properly in our customers' production process.(Frequency of occurrence = 1 per 500)
When the TRF7970A in power down mode (EN = 0, EN2 = 0) under card emulation mode,without touching the IC
card to the reader, IRQ is asserted.There is no RF field.
IRQ is not output when I separate connection between MISO/EN/EN2 pins and MCU physically.It operates correctly
when the TRF7970A replaced with another TRF7970A device.
Is there something that is considered to be the cause of that?
How can the customer work around this issue?
Best regards,
Seishin