Other Parts Discussed in Thread: TRF7970A
Hello
We are trying to make a 4W hf power RFID reader based on the design described on the application note from TI
(See the attached file1488.appnote_trf796x_pwramp_4w.pdf). Basically I have followed the description and the schematic, used the same components etc. We can now read the tag ,but the read range is about 10cm (it is 40cm in the attached file ). The tag and antenna in the picture
. they work well with the TRF7970A EVM modul ( the read range is about 20cm when 200mw mode was set ). I have changed the "Regulator & I/O control register" from 0x87 to 0xC7.
After a long investigation of the whole circuit we did not find any way out to overcome this problem. Please suggest me what to do.