hi,
I'm working with trf7970A. I'm using Spi with SS and ISO15693. I write the register 0x00 -> 0x20 and 0x01->0x02 to work in rfid mode.
I can read all the register.
When pass the tag and read the fifo status, this send me differents value all the time. This is normal? should be a fixed value?
I'm reading a 0x40 in irq status.
I'm using the tag-it HF-i.