This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Getting output on a cc2538 code

Other Parts Discussed in Thread: CC2538, CC1200, Z-STACK

Hi,

   I'm using SmartRF06 EB with cc2538 and also cc1200 connected to the board. I have loaded the spi_master program into cc2538 using IAR workbench. Flashing got over successfully. Now how can I see the output the program? the program is having UARTprintf commands. where i should check for the printed values and is there any connections to be made on the SmartRf board other than GPIO connections with cc1299 to enable UART channels?  

-Thank you