I have a question about HF RFID. Do we need a matching circuit for HF RFID? NFC antenna needs a matching circuit and it is at the same frequency 13.56MHz. So I’m wondering if it is needed for HF RFID. But LF RFID at 125KHz or 134.2KHz doesn’t need it. If a matching circuit is not necessary for RFID regardless of the operation frequency, then is the fundamental difference between NFC and RFID antennas at 13.56MHz?
Thank you,
Jay