Other Parts Discussed in Thread: CC2650
Problem: When running the sblAppExexe, the PC application(sblAppEx) shuts down after selecting the index of the serial port connected to the CC2650EM under test. The EM board seems to be in the bootloader mode after Reset with Select pin held low on the SmartRF06 board. The program is printing something after it tries to connect, but it shuts down before I can read anything.
Setup:
1. SmartRF06 evaluation board with a CC2650EM module, it has the Central application loaded.
2. On my PC I am running the sblAppEc.exe application to test the bootloader commands. I did not build the application, so am using the executable.
3. Enter bootloader mode by holding Select Pin while resetting the SmartRF06 board with the CC2650.
4. I checked the CCFG setting of xC5 using the SmartFlash programmer.
Do I need to rebuild the sblAppEx project to use it with my device, or to adjust the baud rate?
Thanks,
Dan