This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Classical Comissioning Problem, if several Devices at same time wanna join.



Hello there,

Im working on a lighting-network with CC2530, therefore I use the given ZL-Gateway and the Zlight2.  

Im Running the Gateway on a Raspberry Pi. And the Samplebridge-Software on CC2530. It works fine!

We Use the Classical Commissioning-Process to connect the Zlight2. It is working fine, for 1-4 lamps.

And now the Problem:

If more lamps are switched on at the same time (and try to Join the network imediatly via classical commissioning) it only connects a few. sometime 3, sometimes 5. Just like its randomly...

Is there too much traffic on the channel or why does it not work?

My thoughts are that the Zlights has connection conflicts... If more lights asking to join the bridge at the same time???! Maybe the Bridge is to slow?

Thanks in advance!!!!!!

best regards

Rafael