Other Parts Discussed in Thread: CC430F5137, CC1101
Hi,
I want to upgrade fromCC1101-MSP430F5529 to CC430F5137 based platform for miniaturization. CC1101EMK433 module was used along with the MSP430 launchpad in the former case and the carrier frequency was programmed for MedRadio Band (401-406 MHz). Unfortunately, eval. module for CC430 at 433MHz is not available. To design a custom PCB for CC430, can the reference design of CC1101 at 433 MHz be used for designing the rf matching circuits? Will this still allow me to program the radio in the desired frequency range? It would be of great help if someone can provide the BOM and reference design files for CC430F5137 that can operate at 401-406 MHz.
Thanks