This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Smart RF studio 7 (2.3.1) and multiple CC-Debuggers



Hi,

I'm running Smart RF studio on Win 8.1 which is quest in Virtualbox. 

I'm not able to use two CC-Debuggers simultaneously. only device which is connected first is usable. Smart RF studio shows that only one device is connected. Both debuggers can be used independently and also together with Smart RF Flash programmer.

Can someone confirm that it is possible to use multiple CC-Debuggers with same type of SoC in Smart RF studio?