This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can I connect CC debugger to CC2500 device without a adapter board?

Other Parts Discussed in Thread: CC2500

Hi Sir/Madam,

I would like to access to the CC2500 chip on my device and communicate with it through CC debugger. I have read the CC debugger user's guide and noticed that it is possible to connect the CC2500 device with CC debugger through a adapter board. However, I have no any adapter board on my hand now. I am wondering if it is possible to connect my CC2500 device directly to CC debugger? If yes, could you please tell me which pins are needed to connect?

P.S. The pin definition of the CC debugger on my hand is as below:

1 TDO/TDI                                         2 VCC_TOOL

3 TDI/VPP                                         4 VCC_TARGET

5 TMS                                                6 N/C

7 TCK                                                8 TEST/VPP

9 GND                                               10 UART_CTS/SPI_CLK/I2C_SCL

11 RST                                              12 UART_TXD/SPI_SOMI/I2C_SDA

13 UART_RTS                                 14 UART_RXD/SPI_SIMO

Thank you very much for your time!

Best Regards,

Yaqin