This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LF base station schematics, external power supply



We have bought an eZ430-TMS37157 Development Tool, and received together an LF base station (what is the reference?). According to the user's guide SLAU281B, it is possible to use an External Power Supply (Optional) (6.1.1). We have spent a long time searching R34 and R35 on the board, before we realized that the Base Station was improved... The schematics are not up to date, two Diodes D4 and D5 are present and allow to use the power connector without modifying the board. Could you please update the documentations ?

Thank you