Hi,
I am using NFClink to read 156930 tags using a combination of MSP-EXPF5529 + TRF7970ATB. Is there a way of transferring NDEF data via ez430 rf2500 wirelessly to PC. What modifications should i make in the program?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using NFClink to read 156930 tags using a combination of MSP-EXPF5529 + TRF7970ATB. Is there a way of transferring NDEF data via ez430 rf2500 wirelessly to PC. What modifications should i make in the program?
Hi Lakshmi,
I presume you are referring to the Stollman NFCPlayer (version 1.0.153.5) right?
There isn't much in place for doing what you are discussing with that GUI and firmware.
If you try using our firmware example from our Reader/Writer app note: http://www.ti.com/lit/an/sloa227/sloa227.pdf , then I think you may have more options.
The GUI which you can install from that firmware package also generates a .hex file in your PC local folder which has the NDEF data read from tags.
You could then use this file to send the data over wireless from your PC with the EZ430-RF2500 to another device/PC.
That example works with the exact same hardware as you have, so you are good on a hardware aspect!
Hello Ralph,
Is the hex file RW_P2P_CE.hex or is it some other file pertaining to the NDEF message. Also when I tried to configure my cc2500 as linkto and linklisten in simpliciTI. The Leds haven't stopped blinking like it says in the SimpliciTI sample application user guide
Best Regards
Lakshmi
Hi Lakshmi,
Presuming it is installed in default Windows directory, you will find the .hex file I was referring to at:
C:\TI\msp430\TRF7970A_RW_1.02.05\tools\TI NFC Tool\TI NFC Tool\bin\Debug
It is named ndef.hex
You can confirm file contents by using a Hex viewer program like HxD.
Regarding the SimpliTI kit - we have no idea about that EVM at all, you would need to ask about those issues in another forum. I think perhaps this may be the right one? e2e.ti.com/.../156