Hello everybody, I'm a beginner in Zigbee network. I have some questions about IC CC2530.
The CC2530 is fully compatible with Xbee protocol?
In my schematic, I use an Atmega162 and I send data to Xbeepro module via the UART1 of Atmega162 .
Can I do the same thing with ic CC2530? Can I use the same Atmega162 and I send data in USART1 or USART2 of ic CC2530
Can I replace a module Xbee pro by this component?
Can I program or define it as I want?
Best regards.