I have questions about NFC antenna design,
Could you give me links into: application notes, sites or software.
p.s.
I need design PCB antenna with maximum dimension 30 mm x 30 mm.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have questions about NFC antenna design,
Could you give me links into: application notes, sites or software.
p.s.
I need design PCB antenna with maximum dimension 30 mm x 30 mm.
Hi Lukasz,
Here are a few application notes to look into:
1. RF430CL330H Practical Antenna Design Guide
2. Antenna Matching for the TRF7960 RFID Reader
Thanks,
Caitlin
Hi Lukasz,
Attached is a tool you can use for your antenna design. It calculates the inductance of an antenna depending on user defined width, height, number of turns, and trace size of the antenna. A good inductance goal for NFC antennas is around 2 - 2.5µH. Also, the thicker the trace, the better performance of the antenna.0871.Calculate_L.zip
Thanks,
Caitlin
Lukasz,
To add to what Caitlin said, 2-2.5uH is a good value for tag antenna(RF430CLxxxx, RF430FRL15x). Transceiver antenna, such as TRF79xxA should be around 1 - 1.5uH. The correct inductance helps with finding reasonable tuning values and Q adjustment.