This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC debugger sw_redect only recognizes 5 flasher



Hi all,

I am building a programmer unit with 7 CC debuggers. To be able to program a PCB, the LED on the CC debugger flasher needs to be green. When the LED is red, the flasher needs to be reset. Resetting the flasher is possible by pushing the "reset" button or via an executable "sw_redetect.exe" (found in this topic).

When i connect all 7 CC debuggers to my computer, the "sw_redect" tool only recognizes 5 flashers. When i disconnect two of the flashers in the list of 5 flashers and run "sw_detect" again, all 5 connected flashers are listed so its not a USB connection issue.

I want to be able to reset the flashers automatically. So either i have to adapt the flashers electrically with a relay or use a software solution ("sw_redetect").

Is there a solution or workaround for the "sw_redetect" 5 device limit?

Thanks in advance,

Stef