After deleting the Flash inside my application, I can't connect to it anymore.
So I tried to do a mass erase with SmartRf Programmer 2 1.7.3 with the following result:
>Initiate access to target: XDS-06EB12202738A. >Failed to read target memory. >Error while reading memory range. Address 0x40091090. >Start flash erase ... >Erase finished successfully. >Reset target ... >Reset of target successfull.
It says "successfull", but the cc1310 is still not erased and I can't access it. Same result with XDS200 and XDS100v3.
Quick help would be appreciated, before I have to solder a new chip.
Regards, Armin