This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Coding problem

Other Parts Discussed in Thread: CC2430

Hi,

i am using the CC2430/2431 EMK for the purpose of location detection application.

1) Can anyone tell me where i can find the codes that are used to program the reference and blind nodes. I could only get the hexfiles from the Texas Homepage.

2) Is it possible to modify the code needed to program the nodes ?

My intention is to program the reference nodes so that instead of sending the RSSI values to the blind node, it will send the data to a seperate microcontrollor which i will program to calculate the postion of blind node.

This is because i am using a set of accelerometers and gyroscopes to improve the efficiency of lication detection system, and will fuse the data from them and the RSSI values to find the location of blind node.

3) Is it possible to interface the nodes with another microcontrollor other that the smartRF board?

Please help asap.

Thanks