It's hard to describe exactly what I did before my two SmartRF06 boards stopped being recognized as debuggers, but I remember upgrading firmware in SmartRF Programmer v2 (I think this was on the CC1310 launchpad , though), and having several CC1310 in bootloader connected via FTDI vcp chip.
Status right now:
- Both SmartRF06 Evaulation boards only shows up as "USB Serial Converter" in device manager. If I tick "Load VCP" in its properties a virtual COM port also shows.
- No XDS100v3 debugger showing in Device Manager
- I actually had a CC1310 with FTDI vcp chip show up as Texas Instruments XDS110 debugger when connected via serial bootloader. How can this happen?
But how do I restore my SmartRF06 evaluation boards?