This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: Z-Stack 3.0 (Zigbee 3.0) example for ZigBee Light Link Development Kit

Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK

Hi @ all!

I'm trying to build a RGB LED light on the basis of the ZigBee Light Link Development Kit (CC2530ZDK-ZLL). The example project based on the "Z-Stack Lighting 1.0.2" called: "SampleLight - Zlight - Router" works flawlessly.

But I need an example for using the new Z-Stack 3.0 (Zigbee 3.0). Is there any sample project I can directly use with the Zlight hardware to control its LEDs?

I only found examples for the CC2530DK hardware, which has a display and several buttons to enter some settings. The simplistic hardware of the zlight isn't able to do such things. So I just need a software to directly start the touch link procedure.

THX in advance!