Hi
I would like to create a network like this:
One master
four slaves
Master can broadcast a stereo audio stream to all slaves.
One of the slaves can stream a stereo channel to master
Master to slave and slave to master streaming need to happen simultaneously as well.
From chip's documentation this sounded like a possibility. However my wireless configuration does not seem to allow me to set the slave count to 4 when I select 'Stereo bidirectional base station' option under Bidirectional application role. I cannot understand why it has to limit the slave count to 2 in this case.
Appreciate any help on this.
Thank you