Part Number: CC8530
Hi
I would like my CC8530 based slave module to power down when both of the following conditions are met:
1. No input signal for X seconds
2. Master is not transmitting any audio
My current configuration using wireless configurator powers down the device if either of the above are met. That is, the module powers down after X seconds of input silence even if it receives audio from master. This is not that helpful. I appreciate if some one can let me know whether this limitation can be overcome.
Thank you