Other Parts Discussed in Thread: CC2538, CC2592
My application code is to be run on a custom design based on cc2538 and cc2592. The application code executes just fine and i can step into the code at any point.
Because the custom design makes use of Internal 32kHz OSC ,as opposed to External 32k Crysral in 2538EM, I do not know how can I test the RF performance using Smart RF Studio.
Testing with SmartRF Studio, I do see transmission and reception happening but I am not sure if internal 32k rc osc should be/can be set in the smartrf studio.
Any help would be appreciated.