This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP-7970ABP: Energia library for to interface TRF7970A NFC booster pack with CC3200.

Part Number: DLP-7970ABP
Other Parts Discussed in Thread: ENERGIA, CC3200, TRF7970A

I am trying to interface TRF7970A NFC booster pack with CC3200 Launchpad using Energia.Is there any library or example program to which I can refer to. Also, I tried to run the example software provided on the NFC Transceiver Booster Pack page and after a few modifications, the program compiled with ccsv7, I was able to run the program but no card was detected. Is there any way to find out if there is a fault in the hardware of my booster pack?