Hello guys
I'm currently working with TI-cc2530 zdk and trying to attach a analog sensor to smartRF05 EB.
As I studied, 8 pins of P0 in cc2530EM can be used as ADC.
But I just have no idea where are those pins on SmartRF on EB.
I think P0 of EM is connected to some pins(Ports) of EB.
The version of SmartRF EB is 1.8, and what I want to know is which pin is connected to P0 of cc2530EM.
I think this is so basic question so anyone can easily answer on this.
It would be very thankful if you give me any other additional information.
for example,, those information is in which document, or some tips when connecting GPIO.