Part Number: CC2500
Other Parts Discussed in Thread: MSP430FG4618
Good morning,
I'm trying to set CC2500 for continuos transmitting data streaming operations. The transciever is connected to MSP430FG4618 through 4-wire SPI and 2 TTL lines on GDO0 and GDO2.
I read on the Application note that the 2 TTL lines shall be used one as a clock and the other one as data output.
My question is: GDO0 and GDO2 shall be set as output port in order to provide the clock and the data stored in txBuffer to CC2500? Because I saw in the examples code that there is a funtion called "halUartSetup", but I canìt understand what this function is used for, given that the MCU and the trasciever are connected via SPI.
Thankyou very much for your help.
Best regards,
Matteo