Hi, is the Linux driver or software is availale to support the RemoTI-CC2530 RF3CE kit?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The RemoTI RF4CE protocol stack is only built by the IAR compiler, and from their website, it does not look like it runs on a Linux box:
To install and run the IAR Embedded Workbench, you need the following:
If you want to write a sample application for the RemoTI stack on Linux, you would load the pre-built RNP sample application into a CC2530 or CC2531 and communicate via UART or USB (which implements a CDC and mounts as a virtual COM port using standard Linux drivers.)