Part Number: TMS37157
Hi, Can someone tell me the function on NPOR pin on TMS37157. Can it be controlled through an LF Command, so that i can reset a microcontroller through LF command just in case if it gets hang.
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear subin s -
please first see pin description on page 3 of the datasheet, then page 42 in same for the schematic, for when it is used - 
i think if you send a General Read command to Page 25 of the device (from the LF side), it should generate the RESET you can use with the MCU
Hi Josh,
I use PalFi Kit as reader for testing , i found page 25 is not accessible through GUI. Also TMS 37157 datasheet has no reference to Page 25. Pls suggests me how can i access Page 25. Is it possible with PalFI development kit?
thanks