Other Parts Discussed in Thread: CC2500, CC2510, CC2592, CC2590, SMARTRFTRXEBK, MSP430F5438A
I am having difficulty finding a general purpose RF transceiver.
In a nutshell, I am trying to find a general purpose RF transceiver chip which can communicate with an MCU via an SPI, UART or parallel port interface. Therefore I am looking for an RF chip that can send and receive data through radio frequency and can relay its information to an nearby MCU via the mentioned interface standards. Please refer to attachment.
The RF transceiver when paired with the MCU is defined as a unit. Eventually I am looking to adapt 2 or more units to form an RF mesh network where the units can communicate with themselves.
THE PROBLEM:
I have looked into dev kits like:
CC2543-CC2544 Development Kit
and this is an overkill for me and doesn't fit into my actual design. The RF transceivers that I am looking for are without an embedded communication protocol. I've also looked into, zigbee, xbee, Digi, Synapse ect... and all come with a pre-loaded communications protocol which communicates to a central dongle which is connected to a computer. I see the beauty of such a setup since one can use the graphical interface to access every radio for addressing and MCU programming purposes. But my environment does not require such a convenience.
Therefore, the general purpose RF transceiver chip I am looking for will simply send and transmit data based on the instructions my MCU will provide to it. This means that the MCU that's connected to the RF transceiver will have its own communication protocol. Additionally, the MCU will receive its own commands from my proprietary system as shown in the attachment.
REQUIREMENTS
If possible, the transceivers should work with a 2.4GHZ frequency band and allow for a minimal communication distance in open air of between 1000 and 2000 ft. In the future this distance may need to increase. A 250kbs RF data transfer rate or greater is fine. These radios may be installed in homes or commercial environments. For initial prototyping purposes we would need it to be in a PDIP package if at all possible. I will need the datasheets to the RF transceiver part along with the bill of materials and schematics for the PCB antenna dimensions and all the components that may be required for the part.
The RF transceiver chip should consist of minimal amounts of pin outs and a minimal required amount of external components. Therefore, pins for a chip enable, transmit enable, receive enable along with a few other pins for the coil and/or for the crystal attachment if necessary would be perfect. I've used RF "transmitters" (RX or TX) in the passed in an 8 pin dip. This would be very useful for me if Texas instruments would have a "transceiver" (RX AND TX all in one chip) with this sort of simplicity.
Also if there are any development kits for this sort of simple transceiver, please provide links.
All help or feedback is greatly appreciated!
Thank you Texas Instruments for your help and your support!
Robert