Hello,
I am looking for a RF solution which communicates at low speed (38.4k) in house over 40m range. FCC forces me to reduce power when going lower in frequency (-20dBm at 315MHz). My question is: how to design a communication system which meets FCC and 40m in door range? Does FCC only spec the TX power? I see also that FCC specs the RX bandwidth e.g. for 915MHz to 523kHz for 38.4kbaud in DN006. Why do I have to reduce my sensitivity at the receiver by increasing the bandwidth?
Thanks for your help,
Hans-Günter