Other Parts Discussed in Thread: CC2541
Hi,
It seems there are two ways for Frequency and Channel Programming in CC2541 (as described in chapter 25.5 Frequency and Channel Programming)
1- For normal transmit and receive tasks, the carrier frequency is set by using the PRF_CHAN.FREQ register.
2- If PRF_CHAN.FREQ is set to 127, and for the RX and TX test commands, the frequency must be programmed directly in hardware registers.
My questions are:
1- What are the main differences between these two ways of frequency programming?
2- Should LLE be idle when using either way to select a frequency?
3- Which way is the faster way to change channel?
Thanks