Other Parts Discussed in Thread: TRF7970A
Our design uses the TRF7960 in a RFID reader that is located near some high energy subsystems. In our design EN and EN2 are tied to microcontroller GPIO lines. EN2 is kept high and EN is toggled to turn RF on and off. Occasionally the customer has reported that the RF field has turned off and they think it may be due to noise induced by the high energy system. The question is if EN2 glitches down to 0 and back to 1, do we have to go back to EN=0, EN2=0 to get the device back into a known state? Are there any constraints regarding the timing of this?
Thanks.
Steve