Other Parts Discussed in Thread: CC2591, CC2530
Hi experts,
As far as I know that, if I want to extend the range of CC2530, I can use CC2591 range extender and CC2530+CC2591 combination layout shows that the both chips are attached to execute the operation. I am wondering if there is any option to have the flexibility of using CC2591 as an external device (not fully attached to cc2530) so I can plug it in and out whenever needed. It would work like an USB device. When I want to extend the range I'd plug it and when not, I'd remove it. Thanks for any help.