Other Parts Discussed in Thread: CC1350, , CC1310
Hello community member,
Would you please guide on to choose the suitable chip set & wireless network to cover more than 2-3 KM area which consists of multiple high rise building of 20-25 floors.
This area will have around 3000+ sensor nodes interconnected with each other with multiple collector/Hub nodes, collector node should be connected to cloud via WiFi router & send sensor reading as and when it arrives.
The data from the sensor is not time critical but should reach out to collector with reliability, sensor may sends few bytes of data in every 15 minutes to 1 hour.
I've gone through multiple blogs in this community and learned that CC1350 (Sub 1 GHz) is having good coverage of KMs, but can collect data from max 50 nodes ( in secure mode), whereas CC2650 (Zigbee) is having better ability to connect more nodes in the network, but complex to implement, and may take longer time to route the message.
I can see my use case can be realized by both the technology causing lots of confusion to select the appropriate chip set for building this use case.
Your direction would really help on taking further steps to build use case. Please suggest if there is any better solution apart from above. Also guide on building network topology / best practises to avoid network congestion caused by 3000+ nodes. Any reference/ white paper would be helpful.
Considering me novice to wireless domain, pl. suggest better approach to take the leap forward.
Thanks!
Kumar