This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RF430FRL152H: Is there an external antenna for Texas Instruments RF430FRL152HCRGER no more than 10 * 10 mm?

Part Number: RF430FRL152H

Hello!

It is necessary to make a medical transponder using a chip RF430FRL152H. As I understand it for the full operation of the transponder, I need to attach the antenna to the chip? Or  the chip can work from antenna of the reader? And then I do not need to connect the antenna to the chip. Or it is possible that the antenna is already in the chip? But, if the antenna is needed, then how to make a suitable (no more than 10 * 10 * 4 mm). Either tell manufacturers or companies that make similar antennas.

In addition, there is a question about the current at the outputs (GPIOS) of the chip.  What current will be output when running in the active and passive modes? 

I will be grateful for any information that will help me understand this topic.