Other Parts Discussed in Thread: MSP430F2274, TMS37157, LM2767
Hi,
I recently bought the EZ430-TMS37157. My idea was, to switch of the on-board MSP430F2274 via software (all GPIO to input, WDT off, LPM4) und use the TMS37157 with an external circuit.
A part of my external circuit needs 12V (just a few milliamps), so I throught it's a good idea to use two LM2767 voltage doubler in a series to do that.
The first one does a perfect job. I got a little more that 6V.
But when I add the second LM2767, the whole VCC chain brakes down. All signal shows just 3V ripples.
Any idea why?
Kind regards
Gerd